Part Number: ADC12DL500
Other Parts Discussed in Thread: ADC12DL3200EVM
Tool/software:
Hello,
I need a development board that includes the ADC12DL500 ADC chip.
During my research, I came across the ADC12DL3200EVM evaluation board.
The Gerber and design files for this board have already been shared. I believe that if I manufacture the board and mount the ADC12DL500 ADC chip on it, it should work.
According to the ADC12DL3200EVM User Guide, all SPI register configurations for the ADC are done via USB using the HSDC Pro software.
I also own a Xilinx AC701 FPGA development board. However, the FMC interface of the ADC12DL3200EVM is not compatible with the AC701's FMC connector.
I have two main questions:
- If I mount the ADC12DL500 onto the custom-built ADC12DL3200EVM board, will I still be able to configure the device using HSDC Pro software via USB?
- I am planning to design an adapter board to make the FMC output of the ADC board compatible with the AC701. Would such a board introduce any signal integrity issues, particularly for the LVDS lines?
Any suggestions or experiences regarding this would be greatly appreciated.