Part Number: AFE4490SPO2EVM
Tool/software:
So the boards I bought off Digikey apparently are preloaded with v1.3, and I saw that the latest firmware is v1.4. I wanted to update all of them to v1.4 to make sure I have the latest firmware. I was able to update 2 boards before I started getting the below error (VIA 0xBFFF0016). I don't know why it would let me update boards some first, and I get this error on multiple laptops. I even tried updating my VISA driver without any success.
I'm using the TI provided AFE44x0SPO2EVM GUI (version 2.4)
Does anybody know what's going on and how I can fix this? Is there another way to update the firmware? I see the command in the Message Communication Protocol v4.0 (copied below), but it only tells me half the story, saying the "PC will invoke the user interactive executable", so I assume it must be paired with the TI GUI to work.