Part Number: AMC131M03
Other Parts Discussed in Thread: ADS131M04
Tool/software:
Hi im using AMC131M03 IC, in that im facing an issue i have configured data for 16bits , dcdc enabled and OSR of 128 , all are working fine. but sometimes my crc is not matching lets say once in an 300 or 400 reads, during that time im getting an value in status register is 0x0203 , which means last channel data is not ready and word length is showing 32 bits and reset bit is 0 showing no reset occured.
during when my crc is correct , my status register is showing 0x0407 , always which means all channels data are ready, word length is 16bit and reset bit is 1 indicating reset is occured.
but this is happening once in every some 200 to 400 between reads and and after that again some 200 to 400 times crc is matching , what could be the reason. what that reset bit indicates in status register and what is the use. during continuous reading what value that reset bit should be.
can someone suggest how to rectify this. during all these check im not giving any input to channels of ic , im just trying to read and write and verify the crc

regards,
srinath