Other Parts Discussed in Thread: ADS8900B,
Tool/software:
Hello
I'm using the ADS8328IBPW at VA=5V, VBD=2.5V, REF+=4.096V, REF-=0V
From data sheet, SPECIFICATIONS : TA = –40°C to 85°C, +VA = 4.5 V to 5.5 V, +VBD = 1.65 V to 5.5 V, VREF = 4.096 V, and fSAMPLE = 500 kHz
VIH High-level input voltage , 5.5 V ≥ +VBD ≥ 4.5 V , 0.65 × (+VBD) +VBD + 0.3
1. Why in the test condition the 5.5 V ≥ +VBD ≥ 4.5 V and not 5.5 V ≥ +VBD ≥ 1.6 V
2. If the VBD in my design is 2.5V when VA is 5V, the VIH can be > 2.5V ?
Roi