Tool/software:
What is the bandwidth of this DAC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lauren,
We do not have bandwidth characterized for this device. Is the customer trying to produce a waveform of a specific frequency?
Best,
Katlynne Jones
Yes, 50kHz to 150kHz. Will the device limit the bandwidth and cause distortion?
Hi Lauren,
Is this a sine wave? How many points do they want per period, and what SCLK frequency are they using? There are 16 clock cycles per DAC update, so they can write a new DAC at a rate of 1.25MSPS (20MHz/16).
The max number of points per period to get a 150kHz sine wave is 8. (1.25MSPS/150k). I don't see the output buffer having any issue with this speed, but an 8-point sine wave itself would cause a lot of distortion.
Best,
Katlynne Jones