Hello TI Support,
I'm using the DAC8551 in an application where:
-
VREF = 5 V
-
VDD= 5 V
-
VFB is externally connected to VOUT, as recommended for voltage output mode.
Based on the datasheet (section 7.3.1.2), the internal output amplifier has a 2× gain, so the expected output is:
VOUT = 2 ×( DIN / 65536) × VREF
However, I observe the following behavior:
-
For DIN ≤ 32767, VOUT behaves as expected.
-
For DIN > 32767, VOUT suddenly drops to 0 V or becomes unstable.
My Questions:
-
Is this behavior expected due to the fact that
VOUT
attempts to exceedVDD
(i.e., >5 V) because of the 2× gain? -
If so, is reducing VREF to 2.5 V the recommended solution to safely use the full DAC input range?
-
Is there any internal clamping or protection behavior that causes the output to go low instead of just saturating at VDD?
-
Are there any stability considerations with VFB = VOUT that I should account for?
Any clarification on this would be appreciated.
Thanks in advance!
Best regards,
Danidu.