This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8551: DAC8551 Output Issue When VDD = VREF = 5V and VFB = VOUT

Other Parts Discussed in Thread: DAC8551

Hello TI Support,

I'm using the DAC8551 in an application where:

  • VREF = 5 V

  • VDD= 5 V

  • VFB is externally connected to VOUT, as recommended for voltage output mode.

Based on the datasheet (section 7.3.1.2), the internal output amplifier has a 2× gain, so the expected output is:

VOUT = 2 ×( DIN  / 65536) × VREF

However, I observe the following behavior:

  • For DIN ≤ 32767, VOUT behaves as expected.

  • For DIN > 32767, VOUT suddenly drops to 0 V or becomes unstable.


My Questions:

  1. Is this behavior expected due to the fact that VOUT attempts to exceed VDD (i.e., >5 V) because of the 2× gain?

  2. If so, is reducing VREF to 2.5 V the recommended solution to safely use the full DAC input range?

  3. Is there any internal clamping or protection behavior that causes the output to go low instead of just saturating at VDD?

  4. Are there any stability considerations with VFB = VOUT that I should account for?

Any clarification on this would be appreciated.

Thanks in advance!

Best regards,
Danidu.