Part Number: DAC7811EVM
Other Parts Discussed in Thread: DAC7811, OPA2277
Tool/software:
Hello,
Can you please clarify what the minimum required power supplies are to operate the DAC7811 EVM? From what I see in the forums, there seems to be some discrepancies between what is printed in the DAC7811 EVM datasheet and the required supply.
My configuration:
Two DAC7811 EVM connected in a daisy-chain.
The bottom board has W2 in the 2nd slot. The top board has W2 in the 1st slot.
W3 is connecting 1-2 (the left 2 pins) on both boards.
The switches are set to the left on both boards.
Please note, I am not married to this configuration and if there is a better way to demonstrate a minimal viable product, I would be happy to adjust these settings. At this point, I am just looking to verify my driver code is working. To be clear, my question is, what are the required voltage levels on J3 such that an analog voltage would be visible on J1.4 and J1.6?
Thank you for the assistance,
Ray