Tool/software:
Hello,
This is Ken Cui(ken.cui@nxp.com) from NXP semiconductors, and I have a related question about DAC1282 in DC mode.
Given that: AVDD=2.5V, AVSS=-2.5V VREF=5V
by sending a command with 0X24027FFFFF Total of 40 bits data frame, do I get VOUTP = 1.25V, VOUTPN=-1.25V or VOUTP =1.15V and VOUTN=-1.35V refer to AGND?
Another words, is Vcom(-0.1V) applied when in DC mode.
Thanks
Ken
Hi Keith,