Dear Sir,
I am designing a new board using ADS1230, the ADC will be connected to a load cell of capacity 20,000 Kg.
The output of the Load cell will be around is 0.5mV/V.
Now if I am configuring the ADC as Gain = 128, Speed = 10 SPS and provide Excitation of 5V, The part will only see a maximum value of 2.5mV at full scale, which is 20,000 Kg.
I want to measure at 1Kg resolution
Is there any way to provide a higher excitation to the Load cell so that the part sees a higher voltage at its input?
Is there any schematic available for such kind of design.
Regards,
Sam