This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3422: Can I connect a LVDS clock directlly to clock pin?

Part Number: ADC3422

Tool/software:

Hi,

My ADC3422 test PCB board misses the 100Ω termination resistor and AC coupling capacitor for the LVDS input clock. My LVDS clock is a 20MHz clock output from the FPGA, and the common-mode voltage is 1.25V. Can I power on the board to test whether it can be used? Will this damage the clock input circuit of the ADC?

Regards.