Other Parts Discussed in Thread: ADS7142
Hi Support Team,
I'm experiencing difficulties using the ADS7142.
I'm only using one channel, AIN0 (AIN1 is connected to VSS), with AVDD = 1.8V.
Under these conditions, I can successfully read voltage changes from AIN0 externally. However, my final goal is to enable the ALERT function, so that when AIN0 is less than 0.01V or greater than 1.1V, the ALERT pin will be pulled low.
Currently, the ALERT pin is not responding. My configuration settings are shown in the table below (any register not mentioned is left at its default value).
Could you please help me identify what might be causing the issue?