Part Number: ADC12DJ5200RF
Tool/software:
Hi expert,
My customer used two ADC12DJ5200 for phase calibration. Keep the first ADC12DJ5200 phase unchanged (32000 in phase control word). Then adjust the control word of the second ADC12DJ5200 and move toward the first phase. The phase difference between two ADC12DJ5200 was eventually calibrated to 0.02 ps. However, after 30 seconds of operation, the phase difference between the two ADC12DJ5200 increases to 1.9 ps (there was no operation running during this time). After the second calibration, the two ADC12DJ5200 phase difference can settle to within 0.5 ps. What could be the cause of this problem?
Besides, could you provide the details or applications of the ADC offset calibration correction, specifically background calibration (the datasheet only shows a little bit about how to do this, but do not go into detail on how to configure the registers at each step).
Best Regards,
Ryker