Other Parts Discussed in Thread: LMH6554
Tool/software:
HI,
We use the LMH6554 to drive the ADC as Figure 1,the ADC is ADS4249.The LMH6554 converts the 10 MHz(1V VPP) single-ended signal into a differential signal and outputs it to the ADS4249.The sampling frequency of the ADS4249 is 250 MHz.When we used an oscilloscope to measure the waveform at point B, we observed a 250 MHz high-frequency signal superimposed on the 10 MHz output signal as Figure 2.When measuring point A with an oscilloscope, this phenomenon was not observed.When the 22nH inductor is replaced with a 0-ohm resistor, this phenomenon also disappears.The 250 MHz high-frequency signal appears to be related to the ADC sampling and the 22nH inductor.Please help us analyze why ADC sampling interferes with the measuered signals.

Figure 1

Figue 2