Part Number: ADS131M06
Tool/software:
Hi Team,
We received a new ADC request from customer, could you please check below requirements to check if ADS131M06 is the best option?
By the way what is the DNL and ENOB of ADS131M06? I can't find in datasheet.
| [Num. of Channels] | ≥6,support differential input |
| [Resolution] | enob≥16.5,if it is Mux structure, the first sample of this channel, ENOB can be 16.5 and the FSR is +_1 to 2.5V |
| [Sampling Rate] | ≥8ksps,If mux structure, the polling rate should larger than 8ksps |
| [Control Bus] | spi |
| [ADC Architecture] | Sigma-Delta |
| [Integral Nonlinearity] | ≤15ppm |
| [Differential Nonlinearity] | ≤10ppm |
| [SNR] | ≥100dB,typical@50Hz |
| [SFDR] | 参考snr、thd |
| [THD] | ≤-90dB |
| [Analog Input Bandwidth] | ≥1kHz,@8ksps |
Thank you,
Yishan Chen