This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1219: When to Use External REFs: Is an Internal REF Necessary?

Part Number: ADS1219
Other Parts Discussed in Thread: REF6245,

Tool/software:

Hi TI team,

I will use External REF on AIN0, AIN1.

AIN0 and AIN1 connect the differential output of a sensor that operates within 4.5V.

AIN2 and AIN3 are connected to the output of sensors that operate within 2.048V of the internal REF (voltage divider resistor for high voltage monitor, temperature sensor).

Are there any concerns about using external REF for AIN2 and AIN3 as well ?


Best Regards,

Koji