Part Number: ADS1282
Tool/software:
Dear TI team,
I have a question regarding the overvoltage (ESD) protection circuitry on the analog inputs of the ADS1282 ADC. In the Absolute Maximum Ratings section, it is stated that the maximum continuous input current is 10 mA. Does this refer to the maximum current each clamping diode on the analog inputs can safely handle? Would it be safe to apply a voltage higher than AVDD + 0.3 V (for example, 6 V), as long as the input current to the analog pins is limited to a value well below 10 mA (e.g., 100 µA)?
Thank you in advance.