Part Number: ADS1258-EP
Other Parts Discussed in Thread: ADS1258
Tool/software:
I am reading channels AIN0-15 and all SYSRED channels which comes out to 21 channels in auto-scan mode. from the ADS1258-EP datasheet I calculated my sample rate from the following formula:
SPS = Fclk / (128 * (4^(11b-DR) + 4.265625 + TD) * 2^CHOP)
Fclk = 14,400,000Hz
DR = 11b (maximal data rate)
TD = 0
CHOP = 0
SPS = 14,400,000/ (128 * (4^0 + 4.265625 + 0) * 2^0) = 21,365
I calculated the conversion latency from the Calculating Conversion Latency and System Cycle Time for Delta-Sigma ADCs document as follows:
Tcl = x / ODR
Where x is the sinc filter order and got:
Tcl = 5 / 21,365 = 234us
Meaning that the latency for converting all channels should be 21 * 234us = 4914us. However, when I benchmark the software it takes only 2546us and all the samples come out correct.
Here is an example in pseudo code for what is being done:
// Benchmark starts here
CS PIN DRIVEN LOW
FOR CHANNEL in CHANNELS
{
PULSE CONVERT
DO {
CHANNEL READ COMMAND
} WHILE NEW BIT != 1
}
CS PIN DRIVEN HIGH
// Benchmark ends here
Is this ADC's conversion latency lower then the formula or am I getting something wrong ?