This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J60: The ADS54J60 samples plotted in HSDC Pro, the pulse is getting disturbed when the pulse going low to high or vice versa.

Part Number: ADS54J60

Tool/software:

Hi, 

I am giving a 500KHz input signal with 1% duty cycle(20 ns) and the output is as given in image.

And When I give 500KHz input its almost 390-400KHz output signal after plotting. What may be the issue ?

I have checked at the input of the adc, the pulse of 500KHz with 1% duty cycle(20 ns pulse) measured in oscilloscope is fine.

Thank You,

Karthik B N.