Other Parts Discussed in Thread: AFE4950, ,
Tool/software:
is there a registers configuration spreadsheet of afe4960 as the one of afe4950, i get aceess ater signed nda, but cant find a tool to generate register setting.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The AFE4960 does not come with a register configuration spreadsheet like the AFE4950. Instead, the AFE4960EVM includes example scripts that can be used to configure the AFE4960 or modified in order to use custom settings. Instructions on how to run and modify the scripts are included in the User Guide (sections 2 and 6) as well as in Video #4 included in the secure resources.
Regards,
Payton
thank you very much for your quick response, my further question is , how to get a start to setup 4950 with a mcu, if we dont have a spreedsheet tool, with 4950, i can modify the vb code , to generate a array containing all the reg_addr, reg_data
Hello,
To set up the AFE4960 register settings:
1) If you have an AFE4960EVM, you can use the example scripts to help you program the AFE4960, then run the scripts as per the instructions in the user guide, and then export the register configuration by navigating to the "Global Settings" and clicking "Export." This will generate a configuration file you can use as the basis for your own settings.
2) If you do not have an AFE4960EVM, you can go through the register map in the datasheet and set up your register values manually.
Regards,
Payton