This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DL2500: Overshoot & Undershoot on SPI Lines

Part Number: ADC12DL2500

Tool/software:

Hi ALL,

We’re using the LMX2582RHAT in our design, and we’re seeing some overshoot and undershoot on the SPI signals (CLK, CS, SDI). These signals are driven by an FPGA.

Here are the current drive strength settings:

  • SPI_CS#_ADC: 12mA
  • SPI_CLK_ADC: 12 mA
  • SPI_MOSI_ADC: 12 mA

We’d like to know:

  1. is this overshoot & under shoot are within the acceptable limit?
  2. if not, can you please recommend how to reduce them

I’ve attached a signal capture of the SPI clock and the relevant schematic for reference.