Part Number: ADS1115
Tool/software:
Hi expert,
In our design we are powering ADS1115 with 3.3V. In a normal use case, AIN0 and AIN1 pins will have voltage less than 3.3V. However, occasionally they will have 3.8V present on them, which is 0.2V higher than the absolute maximum rating.
Below are the questions we have.
- We are wondering if there is a margin built into this VDD+0.3V maximum rating on the AINx pins.
- Would the AINx pins be able to tolerate 3.8V for a short amount of time (vs a long period of time)? If yes, how long would that be?
Thank you!
McKenna