Other Parts Discussed in Thread: ISO7221M
Tool/software:
Maximum VOL of ADS1235 = 5.25V x 0.2 = 1.05V, Refer Datasheet section “6.5 Electrical Characteristics”
Considering maximum operating voltage.
As we are interfacing ADS1235 with ISO7221 IC which VIL (max.) is 0.8V.
How it will work or Can actual ADS1235 VOL max. is less than specified inthe datasheet?
Kinldy help to resolve the same.