This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7953: ADS7953 Power Sequencing Requirements

Part Number: ADS7953


Tool/software:

Hello!

I haven't been able to find any explicit power-on or power-down sequencing requirements for the ADS7953 in the datasheet. The "Recommended Operating Conditions" specify +VBD should be less than +VA, but the Absolute Max Ratings don't specify any dependency between +VBD and +VA. Is it safe to power on +VBD before +VA is powered?

For reference - in our application:
  +VBD is 1.8V and powers on first
  +VA is 3.3V and powers on <5ms after +VBD
  VREF is 2.048V and will power up simultaneously with +VA