Tool/software:
Hello, we are using ADS7953 to collect the voltage and current values inside the circuit board. There is an abnormality with one of the circuit boards
1. The default state U1 is very hot, 10W.
2. After removing the resistors R1,R2 and R6, they are still very hot, around 9.5W.
VCC_CLK_PLL_D3V3 2.55V
VCC_CLK_PLL_D1V8 1.808V
VDD_CLK_D3V5 3.54V
VCC_CLK_BUFF_D3V3 2.03V
VCC_D3V5 3.53V
VCC_A2V5 2.52V
VCC_A3V3 3.3V
3. Remove U1, the power consumption is 3W, and the voltage returns to normal.
My question is where the problem lies? How to solve it?