Part Number: ADS8681
Tool/software:
Hello,
I would like clarification on the gain error spec of +/- 0.025 %FSR.
Lets take 2 separate cases
1. Unipolar Input Range of 0V to 10.24V.
The gain error at 10.24V input is +/- 0.025% * 10.24V = 2.56mV. I think this is straightforward.
2. Bipolar Input Range of -5.12V to +5.12V.
Is the gain error at 5.12V input also +/- 0.025% * 10.24V (FSR) = 2.56mV?
Thanks,
Stanley