Part Number: ADS1292R
Tool/software:
Dear teams,
When conducting frequency response testing on ADS1292R, one of the inputs is a 2mV, 0.5Hz sine wave and a 2mV, 10Hz sine wave.
Based on 10Hz, the waveform amplitude at 0.5Hz should be within the range of -10% -5% of the 10Hz waveform amplitude.
As shown in the attachment, our test results are not satisfactory, but we have tested the 0.67Hz waveform and it is satisfactory.
May I ask what methods can be used to make this test pass?