Tool/software:
I designed it by applying TXS0104E to UART communication. The UART speed is 460800 baud rate. In the output waveform in the attached figure, the 5V signal is output as 3.2V and is operating as open drain.
I have a question. First, on the datasheet, it is maximum data rates 2Mbps open drain, and all the waveforms are crushed. Why is that?
Second, the input is push pull, but the output is open drain. How do I get the push pull output waveform? I applied TXS0104E to use it for both spi and uart communication.
I'm sure you're busy, but please reply in detail.