Other Parts Discussed in Thread: AFE20408, AFE10004
Tool/software:
Hi, I plan to use AMC7834 to bias a GaN Power Amplifier. I had some queries regarding that:

Here, they have mentioned that the settling time to go from 400h to C00h is 10us. I want to know how long it will take to go from -5V to -2.5V with a step size of 0.5V? (Given, 000h is -5V and FFFh is 0V)- If Avss = -5V, does the thermal pad also need to be connected to -5V?
- What is the frequency of the clock used for DAC? Can we control the clock rate using any software code?
Thanks,
Manik