This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: Output signal distortion

Part Number: TXS0108E

Tool/software:

From 1.8V to 3.3V, the input signal of A/B is normal and stable, but the output signal is distorted , the rise time is too long. What is the reason? The waveform of TX-E to RX_MCU and TX_MCU to RX-E are the same, but the output is distorted.

SCH:

Input: TX_E

Output RX_MCU