Tool/software:
Hello Team,
We are currently using this ADC in our product to acquire four analog signals (AIN0 to AIN3), all of which are connected.
After thorough investigation, we have isolated an issue that appears to be within the ADC itself.
Issue Description:
- In a small number of units, 3 samples out of over 30,000 products, we’ve observed incorrect readings specifically on AIN2 when the surface temperature of the ADC exceeds 65°C.
- AIN2 is configured to measure an amplified current signal.
- We have verified that the analog input to the ADC is accurate and stable.
- However, the digital value read by the microcontroller from the ADC for AIN2 is incorrect, it appears as garbage data.
- The other input channels (AIN0, AIN1, AIN3) continue to function normally under the same conditions.
- Based on our analysis so far, the issue is not with the analog signal chain but seems isolated to the ADC’s behavior at elevated temperatures.
- Could also be an issue with i2c.
- When temp <65 deg, ADC works as expected.
As i had mentioned, we are not seeing this behavior in all parts but only few and in these few issue is reproducible.
Have you seen this behavior before? Could you please support and share the FTA for the same. Thank you