Other Parts Discussed in Thread: TVP7002, THS8200
Hello,
The customer is having some issues with the TVP7002EVM kit. He using an input of 1280 x 768 @60Hz and setting the output to run @ 1080p. His video output looks redish and is constantly scrolling up. The settings he is using are:
System Initialization
(TVP7002 - Switch to EVM VGA Input)
(1280x768x60Hz- 47.8khz - 79.5MHz HS/VSin -/+)
(CSC Bypass)
for the TVP7002 Property Sheet he used the preset settings
for the THS8200 Property Sheet he is not sure what to set the HS_IN_delay and VS_IN delay to.
Thank you,
Alex