Part Number: ADS131M08
Other Parts Discussed in Thread: OPA2992, TPS7A20, LP2985A
Tool/software:
Hi Ti-Team
I have an additional question regarding my circuit with the ADS131M08.

I tested everything so far with the EVM board I have an everything looks fine. At least at room temperature. I will perform a 2-point calibration at 4ma and 20mA in our final product.
My questions are:
How accurate will these values be after 10/20 years?
Can I achieve 0.1% overall accuracy over a temperature range from 0-60°C with the internal reference?
Is the input bias current (3-4µA) about to change with time and if so should I use input buffer (e.g. OPA2992)?
Is the LP2985A (new version) good enough for 0.1% or should I use the TPS7A20?
Thank you in advance.
Regards Theo