Tool/software:
Hi team,
Regarding the output voltage headroom with the specifications below, is it correct to understand that if the current is around ±10mA, the output voltage range will narrow by at least 1V?
If you want to use the full set output voltage range, is it correct to understand that you need to input a Vcc with sufficient margin for the output voltage range?
Also, the output voltage range narrowed by the headroom only affects the upper voltage and does not impact the resolution, correct?
Best regards,
Kyohei