Part Number: DAC39J82
Other Parts Discussed in Thread: OPA818
Tool/software:
我们目前的方案是高速DAC(DAC39J82)+运放(OPA818)输出电压信号,我们想在此基础上再加一级电路(外部加个小电路板)将电压信号转换成电流信号,带宽在500Mhz。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This needs to be translated in order to support.
Regards,
Geoff
Our current solution is to use a high-speed DAC (DAC39J82) and an operational amplifier (OPA818) to output voltage signals. We would like to add an additional circuit (an external small circuit board) to convert the voltage signal into a current signal, with a bandwidth of 500MHz.
HI John,
Are there any additional details you could provide on the output current required. Will it be bipolar or unipolar? Also, the magnitude will be important. For really large current requirements, a larger power mosfet would likely be required which would make the bandwidth requirement extremely difficult.
Best Regards,
Ignacio