This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8686S: Regarding the MUX switching time and settling time of the MUX-integrated ADC

Part Number: ADS8686S

Tool/software:

Hi team,

I believe the maximum sampling rate of this device is 1MSPS, but does this include the switching time and settling time of the built-in MUX?

Additionally, my customer is considering using this device with several power input ranges such as ±10V, ±5V, and 0-30V, varying by channel.

Will additional MUX switching time and settling time occur when the input voltage range changes?

Best regards,

Kyohei