Tool/software:
Hi,
we are observing the following spike seen on the screenshot below. The spike appears when we do the reset (purple line) and we remove +5V power (green) and -5V (yellow). In some of the mentioned DACs and on some channels, we get a positive 0.7V spike added to the normal discharge to 0.
Green: +5.0VA on TI DAC
Purple: Reset on TI DAC
Magenta: Spike in some of DAC outputs
Yellow: -5.0VA on TI DAC
We added a 100Ohm resistor in parallel with the 10uF capacitor on +5V rail which seems to solve the problem with the spike, but due to higher current draw, we are searching for a better solution. Have you observed similar behaviour before and if so, how was it solved?