Part Number: ADC09QJ1300-Q1
Tool/software:
Table 6-16, 6-17 and 6-18 in the data sheet does not show the max for the input clock range for JMODE 5. The non-Q100 version of the data sheet shows this max at 1040 MHz. I'm supporting an application which is interested in using this mode, but needs to support 1 GHz clocking rate.
Is this a typo and should be 1040 MHz?