Part Number: ADC3663
Tool/software:
Hello,
I am using an ADC3663 that is configured as follows and I am currently seeing a severely quantized 16-bit digital output when a continuous triangle wave is applied at the input
1. 2-wire mode
2. 16-bit
3. Default output bit mapping
4. No output scrambling
5. 20 MHz sampling
6. Differential analog input, differential SLVDS digital interfaces
7. No decimation (digital feature block bypassed)
8. Format A & B set to offset binary
The quantizations in 16-bit space are roughly 4,096 counts apart (plus or minus 600 counts). See the capture below.
Both channels A and B look similar.

The test patterns look perfect w/ no sign of quantization (both the ramp and the fixed constant versions). The differential analog input at the ADC inputs also shows no sign of quantization.
What ADC misconfigurations might cause this quantization?
Update - ADC Clock & ADC Input Circuitry / Quantized Output of 2.0V DC Input