Tool/software:
When using ADS1220 for bridge measurement, I use the built-in IDAC for bridge excitation, connected to AIN0/REFP1, and the other end of the bridge connected to AIN3/REFN1.
When converting, AIN3/REFN1 is connected to VSS, and the reference voltage source is built-in 2.048V.
However, I hope to reduce common mode interference and want to change the reference voltage source from the built-in voltage source to REFP1 and REFN1. I wanna to ask if IDAC can be used simultaneously to connect to REFP1 and input REFP1 as the reference source?