Part Number: DAC3283
Tool/software:
Hi
I am using DAC3283 in my application.
DATACLKx = 400 MHz
DACCLKPx = 400 MHz
OSTRx = 1.25 MHz.
FRAMEx = 3.125 MHz
Interpolation = x2
With these configurations, DAC Linkup works, and I can send correct data to DAC. But multi chip synchronization is not working.
The Data sheet states, "The frame signal can be either a pulse or a periodic signal where the frame period corresponds to 8 samples." So Frame clock must be DATACLKx / 8 = 50 MHz

Is it correct to use a Frame clock of 3.125 MHz? Does it effect synchronization?