Part Number: AMC7836
Tool/software:
Hello E2E Experts,
Good day.
I am reviewing the datasheet of AMC7836. For the ADC[0 to 15], it is said on the datasheet that the LSB is 25 x Vref / 4096 (on page 30). That is where I am confused because when the output range is 25 V(-12.5 to 12.5 V) and the 12 bit, the LSB should be just 25 / 4096 = 6mV. Please check the following screenshot for detail.

Regarding the possible error I highlighted in the screenshot, I think the 25 x Vref / 4096 should be 2 x 5 x Vref / 4096.
Regards,
TICSC