Part Number: ADS131M08
Tool/software:
When we were using the ADS131m08, the accuracy suddenly became inaccurate. For instance, when the source output a 5A AC signal, the meter could initially test the correct value of 5A normally. After running for a period of time, it showed 5.08A. When the source output was 4A, the meter tested a value of 4.03A. After troubleshooting, it was confirmed that there was no problem with the source output. At this point, the ADC data conversion rate is not an issue. It has always been the 8K rate we configured, and the SPI data frames captured are also normal. It can be restored after the watch is restarted (the board is powered off and restarted). This phenomenon occurs with a low probability in our area. Currently, we can't find the cause. I would like to ask how we can further locate and investigate it. By the way, the two values mentioned above, 5.08A and 4.03A, are not the results of the default gain value (8388608).