Part Number: ADS8568
Tool/software:
I have read the following questions but they do not solve my problem.
Using software mode(HW/SW pin is '1'.), serial interface(PAR/SER pin is '1'.). The read data is all '0'.
Please let me know about the following questions:
1) The question above mentions CONVST_x, but do I need to drive CONVST_x to a high level to read the Configuration (CONFIG) Register?
As a test, I drove CONVST_x to a high level in sync with reading the Configuration (CONFIG) Register.
Data was output from SDO_A, but I believe this was AD converted data.
2) To read the Configuration (CONFIG) Register, bit 30 (READ_EN) must be set to '1', but at this time, does bit 31 (WRITE_EN) also need to be set to '1'?
3) The description of bit 30 (READ_EN) of the Configuration (CONFIG) Register states "Configuration register contents output on SDO_A with next two accesses," so I am issuing three read accesses via the serial interface. Is it necessary to set bit 30 (READ_EN) to '1' for all three read accesses?
Regards