Part Number: ADS1115
Tool/software:
HI, Staff
An offset occurs
We are testing an analog input interface with 0-10V input using the ADS1115.
An offset occurs in the AD conversion result.
This effect tends to be particularly pronounced when C of a CR low-pass filter is connected.
For example, when AIN0=0V, the AD conversion result is about 1.9mV.
The circuit configuration is that the 0 to 10V input signal is resistively divided to 0 to 3V, then connected to a CR filter (C: 4.7nF, R: 499Ω) and then input to AIN0 of the AD converter.
The CR filter is based on the EVM circuit. Single-ended ±4096mV, data rate is set to 860SPS.
What causes the offset?
Please let me know.
regards
cafain