Tool/software:
Hi! I am considering VSP5610 for a CCD-based spectrometer application.
I would like to get a reference manual containing the register map to set up the timing generator and acquisition settings.
The second question is about the operation of the SPI's input shift register. As the packet length is specified to be 30-bits, which is not a standard length, I am wondering if a 32-bit packet can be used and the shift register would then discard two extra bits or if a custom implementation of the SPI-master is required in this case.
Thanks in advance!