Tool/software:
Please let me know what is effect on DAC38J84 device performance if the input clock signal LVDS instead of LVPECL
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Please let me know what is effect on DAC38J84 device performance if the input clock signal LVDS instead of LVPECL
Hello,
If you use LVDS signal for the DAC38J84, the slew rate of the LVDS signal and also the inherent noise performance may create additional noise due to jitter. This may impact the overall phase noise of the DAC. Please see below two app notes for reference. Thank you!
Hello Kang Hsia,
We are using an RF transformer (Part Number: TC1-1-13MG2+) to convert differential signals for DACCLKP & DACCLKN and the FPGA clock.
Currently, we are observing the NCO signal, but when using JESD, the DAC output is not coming.
Could you please help clarify the issue or provide guidance on possible causes?
Hi
on the datasheet there are recommended clock interface, please follow the instructions and also refer to your clock driver instructions
Currently, we are observing the NCO signal, but when using JESD, the DAC output is not coming.
I am not clear on your questions. There are various posts on JESD debug, you can refer to them as a starting point.