Tool/software:
Hello,
I used the ADS1255 to measure a NTC. The component works and I receive on SPI bus the good value exept during the value 0x00. To proove the issue, I use potentiometer. If a set the position and I don't touch it, I receive the 0x 00 00 17, that it's good and sometime, I received wrong frame with a value of : 0x 00 7F 0x90. In attachement I put both graph.
For me, the soft is good because we can see that the frame change on the SPI.
Do you have an idea why the value converted by the ADC change without change the potentiometer position. The changing is important to be a problem with micro mouvement of the potentiometer.
Thank you
Best Regards