Part Number: ADS9813
Other Parts Discussed in Thread: ADS9803
Tool/software:
hi sir
did ti have the solution which is 20 bit adc/ 8ch adc solution?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
Hope you're well, thanks for your post. We have a 20-bit version of ADS9813, called ADS9803, in the pipeline. It is set to release in the next week or two. I will let you know when it is released. What kind of project are you planning to use it for?
Best regards,
Samiha
HI Samiha
the end equipment is the ATE for Diode tester
now we also survey the ADI/AD4858, Did you have the compare table between two?
thanks
Hi Alex,
Thanks! The main difference is the competitor device has high input impedance (due to internal buffer) and a 40Vpp input range. ADS9803 has only 1Mohm input impedance and 24Vpp input range. If the ADS9803's input range works for your diode tester, our device will offer 2x faster sampling and ~30% more accuracy. I can email you a comparison slide.
Best regards,
Samiha