Part Number: LSF0108
Other Parts Discussed in Thread: LSF0204
Tool/software:
Hi,
I have a few questions regarding the LSF0108 IC.
1. I planned to connect the VCCA = VCCB at same voltage level. Is LSF0108 IC supports same voltage level. I didn't see anything regarding what would happen if VccA= VccB. Please provide your feedback.
2. If the low voltage power rail 1V8_power_A domain in my case is enabled first then there is a long delay before the 1V8_power_B domain rail. Is there are risk of high current flow through the MOSFET body diode and through the target ICs(SoC) ESD TVS diodes? Is there are chance there can be problems in this scenario? please provide your feedback.
3. LSF0108 device supports I2S communication. If yes any preventive measures requirement to take care in design. provide your feedback.
4. LSF0204 device supports IOFF and partial power down mode(attached image for reference)
. Similarly, LSF0108 supports the same features. Please confirm.